I am new on TI MCU's, i installed CCS 6.1.3.00033 and set it for al devices, i am trying to run example from TI Resource Explorer, when i try to run the debug i get error msg:
Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 6.0.222.0)
I am sure that the USB is recognized: