Hi,
We are currently evaluating a SEED DSP.COM XDS560PLUS emulator with CCSv4 and have trouble with the following persistent error :
" C55xx: Trouble Halting Target CPU: Error 0x00000020/-2062 Error during: Execution, Cannot halt the processor "
Effectively it interferes with our debugging process, whatever the reason maybe, as a break-point is NOT correctly processed and the code never stops, not even when activating the halt button in CCSv4.
The XDS560PLUS emulator seems to have been correctly installed as it is recognized by windows. We are using the EVM5505 for target configuration however our target board is a custom built board based on the 5505 DSP.
Any pointers or hints on what could be causing this would be greatly appreciated.
Kind Rgards, M