This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have MSP-FET which according to the debugger guide supports Spy Bi-Wire for MSP430F5342. I am unable however to get it to work, each time I get a communication error even though the wiring is identical to below. Surprisingly, when using the programming dongle for chronos it works without problems. Not sure what is wrong or causing that error. Thanks.
Fahd
By default the MSP-FET attempts to automatically select either Spy Bi-Wire or JTAG mode.Fahd Albinali said:I have MSP-FET which according to the debugger guide supports Spy Bi-Wire for MSP430F5342. I am unable however to get it to work, each time I get a communication error even though the wiring is identical to below. Surprisingly, when using the programming dongle for chronos it works without problems
There have been some other hardware configurations where the automatic MSP-FET SBW / JTAG mode selection failed to allow communication with the device. The thread Forcing SBW mode describes a change to a CCS XML file to allow SBW mode to be forced when using the MSP-FET. Maybe forcing the MS-FET to use SBW mode will help in your case.