This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6000 cgt 6.1.10 documentation ?

hi, because of customer's requirement, i need to use CCS 3.3, which provides c6000 cgt 6.1.10. but the problem is that no documentation for linker and  compiler exist.

1. where can i download the cgt 6.1.10 documentation as pdf?

2. is it possible for me to download the latest cgt which is compatible with CCS3.3 and its documentation?

  • canfoderiskii said:
    1. where can i download the cgt 6.1.10 documentation as pdf?

    From here.

    canfoderiskii said:
    2. is it possible for me to download the latest cgt which is compatible with CCS3.3 and its documentation?

    Please see this wiki article to understand the differences among compiler versions.  You can download more recent versions (not including 6.1.x) of the C6000 compiler from here.  If you decide to stay with a 6.1.x compiler version, then you should know the latest release is 6.1.23.  You may be able to get it with the upgrade feature in CCS 3.3.  I don't know if that still works, but it can't hurt to try.

    Thanks and regards,

    -George

  • thank you for the reply, i have to stay with 6.1.x because CGT 7.x is not compatible with CCS v3.

    I'll try to update cgt to the latest 6.1.23 using CCS upgrage feature later.