This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Signals look different with different sampling frequencies

Hey John,

thanks for your help! I thinks that works now.

But today i notice that if i display a graph with a different Sampling Rate HZ variable, then i got a different signal?

In the following picture i i display the signal one time with 1 Hz Sampling Rate and one time with 100 Hz Sampling Rate.

Why i got there different cycle durations?

Thanks for your awesome help!!

 

regards

thomas

  • Thomas,

    I am going to split the last question into a separate thread as I will need some help on this one.

    John

     

  • Thomas,

    Looks like you have an aliasing problem.  The period from the 100 Hz sample rate is 1.2 seconds which is more that 1/2 the 1 Hz sample rate in the first example.  You need to sample at at least 2 Hz to resolve the signal correctly if it is an aliasing problem.

    Regards.

  • Hey,

    This sounds good, but i checked it and get the same failure.

    The more i increased the value of the Sampling Rate, the period gets lower? for example today i get for the same adjustment another values?! following i post some signal plots of the same signal but with different sampling rates and additionally my settings. The period of the signal should be 1.2 s.

     

    With 10 Hz i get the solution how i visualised it, but i don´t realize why the other outputs are different.

    Thanks a lot!

    regards

    tom