This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v6 install - Error in startup script - twapi.dll

Other Parts Discussed in Thread: CCSTUDIO

Hello,

Has anyone been able to install CCS 6.1.3 on Windows 10 Pro 64-bit?

After starting ccs_setup_6.1.3.00033.exe, it progresses to "installing com.sd.ccst[...].emulation.win32", then shows a dialog.

Thanks for all suggestions.

---------------------------
Error in startup script
---------------------------
failed to load library "/installkitvfs/lib/twapi/twapi.dll": could not load file from temp location: couldn't open "C:\Users\awozniak\AppData\Local\Temp\TCLDBE8.tmp": no such file or directory
    while executing
"load [file join $twapi::scriptdir twapi.dll]"
    (file "/installkitvfs/lib/twapi/twapi.tcl" line 23)
    invoked from within
"::tcl_source /installkitvfs/lib/twapi/twapi.tcl"
    ("uplevel" body line 1)
    invoked from within
"uplevel 1 [list ::tcl_source [lindex $args 0]]"
    (procedure "source" line 3)
    invoked from within
"source /installkitvfs/lib/twapi/twapi.tcl"
    ("package ifneeded" script)
    invoked from within
"package require twapi"
    (procedure "::InstallJammer::LoadTwapi" line 13)
    invoked from within
"::InstallJammer::LoadTwapi"
    (procedure "::InstallJammer::InitInstall" line 7)
    invoked from within
"::InstallJammer::InitInstall"
    (file "/installkitvfs/main2.tcl" line 30300)
    invoked from within
"source [file join $::installkit::root main2.tcl]"
    (file "/in ...
---

Pressing OK does a retry of twapi.dll and finally shows:

---
An error occured : Installer failed to install com.sd.ccstudio.emulation.win32 correctly. The 2 most common reasons for failure are:
    1.  Anti-virus on your computer could have impeded the executable.
    2.  Download is corrupted.
Please submit these logs to TI for analysis using the next dialog.
You may also visit the TI E2E CCS Support forum for additional help.

The install logs are located in: c:/ti/ccsv6/install_logs.
---

The logfile shows:

---
06/23/2016 16:08:09(GMT) - processOtherFeatures - CCS_INFO: binary sd_emupack_setup_5.2.0.14.exe; ext = .exe
06/23/2016 16:08:09(GMT) - InstallBins - .exe: sd_emupack_setup_5.2.0.14.exe --mode silent  --prefix "c:/ti/ccsv6/ccs_base" /noc2400 /noc5400 /noomap /nodavinci
06/23/2016 16:08:09(GMT) - InstallBins - cmd = "c:/ti/ccsv6/eclipse/downloads/sd_emupack_setup_5.2.0.14.exe" --mode silent  --prefix "c:/ti/ccsv6/ccs_base" /noc2400 /noc5400 /noomap /nodavinci
06/23/2016 16:08:09(GMT) - InstallBins - CCS_INFO: Installing com.sd.ccstudio.emulation.win32
06/23/2016 16:08:17(GMT) - InstallBins - CCS_INFO: error message: child process exited abnormally
06/23/2016 16:08:27(GMT) - InstallBins - CCS_INFO: Installing com.sd.ccstudio.emulation.win32
06/23/2016 16:17:51(GMT) - InstallBins - CCS_INFO: error message: child process exited abnormally
06/23/2016 16:18:01(GMT) - InstallBins - CCS_INFO: Installing com.sd.ccstudio.emulation.win32
06/23/2016 16:18:29(GMT) - InstallBins - CCS_INFO: error message: child process exited abnormally
06/23/2016 16:18:29(GMT) - processOtherFeatures - CCS_INFO: Finished installing binary sd_emupack_setup_5.2.0.14.exe
06/23/2016 16:18:29(GMT) - processOtherFeatures - new state: install failed
---