This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1.3 Crashing While Loading Symbol File

Other Parts Discussed in Thread: AM3352

Hi all,

I have been having crashing issues with Code Composer Studio 6.1.3 while attempting to debug u-boot on an AM3352 device. The crash occurs when I try to load a symbol file into memory using the offset data found in u-boot. The offset was reported to be relocaddr = 0x9FF72000. I have attempted to load the symbol file on both Ubuntu 14.04 and Windows 7, both yielding the same results (CCS crashes). I should also note that I was using a custom gel file in the target configuration (I can send the the file if needed). Here is the hardware and software I used (I will stick with Windows for troubleshooting):

Windows 7 Enterprise (Service Pack 1), CCS 6.1.3.00033, AM3352 device, TI XDS100v2 USB Emulator

Any Information you could give on this issue would be greatly appreciated.

Marcus Mueller

0407.CCS_Logs.zip