This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bit mask error



I am seeing what appears to be C2000 compiler bug.  When the C++ code below shown is compiled, it produces a 32-bit write that clears the upper 16 bits instead of ORing them.

Notes:
1.  The struct labeled "fpga" within in gd is a group of pointers that point to a memmory mapped  IO device.  gd.fpga.control->header is defined
    as unsigned long.
2.  If I exclude the "proprietary code" the problem does not manifest.
3.  If I change the two lines labeled "W1" and "W2" to the single line labeled "W3", the problem does not manifest.
4.  The problem is new to CCS version 6.1 tools.  It is not seen with version 5.5.

So it appears the problem is somehow related to optimization, especially given note 2.  It appears to be setting up the registers to optimize for
the code that follows.

When trying to produce a version of a pre-compiled file that doesn't contain a bunch of proprietery code, I observed
the assembly language would take on a 2nd non-working variant;  after reading in the initial 32-bit value to ACC, it  would copy the lower 16 bits to P,
operate on P and then write the full 32 bits of P back to the output.  This had the effect of making the upper 16 bits arbitrary depending on what was  already in P.

Also, I tried writing it without using the local variable "header" and just doing the bit-wise OR directly on the IO register and it produced a similar failure.

Below the non working assembly language code, I've included a snippet of the working assembly code that results from the changes mentioned in notes 2 and 3 above.

The compile line command is:

C:/ti/ccsv6/tools/compiler/c2000_6.4.11/bin/cl2000" -v28 -ml -mt --float_support=fpu32 -O3 --opt_for_speed=3 --include_path= ... -g
--define= ... --diag_warning=225 --display_error_number --rpt_threshold=8 -k --preproc_with_compile --preproc_dependency=".../src/myFile.pp" --obj_directory=".../src"  "D:/xfpWorkspace/2.4/xfp/3L/BaseSoftware/src/myFile.cpp"
_______________________________________________________________________________
C++ source code:

volatile Uint32 ledDebug = 0;
void calc(void)
{
 
    int i;
    static unsigned int counter = 0;

    if(gd.numToAvg) {

        unsigned long header = gd.fpga.control->header;
        if (gd.fpga.control->header&0x00010000)
        {
            ledDebug = gd.fpga.control->header;
        }
/* W1 */        header |= 0x00000020;
/* W2 */        gd.fpga.control->header =  header;  /*** resulting write writes only the lower 16 bits and 0s the upper 16 bits ****/
// /* W3*/       gd.fpga.control->header = header | 0x00000020;


    }
    /***** PROPRIETARY CODE  HERE   *****/
 
}
_______________________________________________________________________________

NON-WORKING Generated assembly code:
        MOVL      *SP++,XAR1            ; [CPU_]
        MOVL      *SP++,XAR2            ; [CPU_]
        MOVL      *SP++,XAR3            ; [CPU_]
        MOV32     *SP++,R4H             ; [CPU_]
        MOV32     *SP++,R5H             ; [CPU_]
        MOV32     *SP++,R6H             ; [CPU_]
        MOV32     *SP++,R7H             ; [CPU_]
        MOVZ      AR2,SP                ; [CPU_]
        SUBB      FP,#16                ; [CPU_U]
        ADDB      SP,#64                ; [CPU_U]
        MOVL      XAR1,#_gd             ; [CPU_U] |14|
        MOVL      ACC,XAR1              ; [CPU_] |14|
        ADD       ACC,#31 << 4          ; [CPU_] |14|
        MOVL      XAR4,ACC              ; [CPU_] |14|
        MOV       AL,*+XAR4[0]          ; [CPU_] |14|
        BF        $C$L2,EQ              ; [CPU_] |14|
        MOVL      ACC,XAR1              ; [CPU_] |16|
        ADD       ACC,#69 << 2          ; [CPU_] |16|
        MOVL      XAR4,ACC              ; [CPU_] |16|
        MOVL      XAR5,*+XAR4[0]        ; [CPU_] |16|
        MOVL      ACC,XAR1              ; [CPU_] |17|
        ADD       ACC,#69 << 2          ; [CPU_] |17|
        MOVL      XAR4,ACC              ; [CPU_] |16|
        MOVL      XAR6,*+XAR5[0]        ; [CPU_] |16| ********  READS FULL 32 BITS FROM I/O REGISTER INTO XAR6    ********
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |17|
        TBIT      *+XAR4[1],#0          ; [CPU_] |17|
        BF        $C$L1,NTC             ; [CPU_] |17|
        MOVL      ACC,XAR1              ; [CPU_] |19|
        ADD       ACC,#69 << 2          ; [CPU_] |19|
        MOVL      XAR4,ACC              ; [CPU_] |19|
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |19|
        MOVW      DP,#_ledDebug         ; [CPU_U]
        MOVL      ACC,*+XAR4[0]         ; [CPU_] |19|
        MOVL      @_ledDebug,ACC        ; [CPU_] |19|
$C$L1:    
        MOV       AL,AR6                ; [CPU_]      ******* COPIES ONLY LOWER 16 BITS FROM XAR6 TO ACC     ******
        ORB       AL,#0x20              ; [CPU_] |22| ******* BIT-WISE OPERATION ON LOWER 16 BITS   *********
        MOVZ      AR6,AL                ; [CPU_] |22| ****** CLEARS THE UPPER 16 BITS OF XAR6     ********
        MOVL      ACC,XAR1              ; [CPU_] |22|
        ADD       ACC,#69 << 2          ; [CPU_] |22|
        MOVL      XAR4,ACC              ; [CPU_] |22|
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |22|
        MOVL      *+XAR4[0],XAR6        ; [CPU_] |22| ****** WRITES THE FULL 32 BITS   ************
        
    /***** PROPRIETARY CODE  HERE   *****/
_____________________________________________________________________________________________________________
    
WORKING Assembly CODE
        MOVL      XAR1,#_gd             ; [CPU_U] |14|
        MOVL      ACC,XAR1              ; [CPU_] |14|
        ADD       ACC,#31 << 4          ; [CPU_] |14|
        MOVL      XAR4,ACC              ; [CPU_] |14|
        MOV       AL,*+XAR4[0]          ; [CPU_] |14|
        BF        $C$L2,EQ              ; [CPU_] |14|
        MOVL      ACC,XAR1              ; [CPU_] |16|
        ADD       ACC,#69 << 2          ; [CPU_] |16|
        MOVL      XAR4,ACC              ; [CPU_] |16|
        MOVL      XAR5,*+XAR4[0]        ; [CPU_] |16|
        MOVL      ACC,XAR1              ; [CPU_] |17|
        ADD       ACC,#69 << 2          ; [CPU_] |17|
        MOVL      XAR4,ACC              ; [CPU_] |16|
        MOVL      XAR6,*+XAR5[0]        ; [CPU_] |16| ********  READS FULL 32 BITS FROM I/O REGISTER INTO XAR6    ********
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |17|
        TBIT      *+XAR4[1],#0          ; [CPU_] |17|
        BF        $C$L1,NTC             ; [CPU_] |17|
        MOVL      ACC,XAR1              ; [CPU_] |19|
        ADD       ACC,#69 << 2          ; [CPU_] |19|
        MOVL      XAR4,ACC              ; [CPU_] |19|
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |19|
        MOVW      DP,#_ledDebug         ; [CPU_U]
        MOVL      ACC,*+XAR4[0]         ; [CPU_] |19|
        MOVL      @_ledDebug,ACC        ; [CPU_] |19|
        MOVL      ACC,XAR1              ; [CPU_] |23|
        ADD       ACC,#69 << 2          ; [CPU_] |23|
        MOVL      XAR4,ACC              ; [CPU_] |23|
        MOVL      XAR4,*+XAR4[0]        ; [CPU_] |23|
        MOVL      ACC,XAR6              ; [CPU_] |23| ******* COPIES FULL 32 BITS FROM XAR6 TO ACC     ******
        ORB       AL,#0x20              ; [CPU_] |23| *** BIT-WISE OPERATION ON LOW 8 BITS    ****
        MOVL      *+XAR4[0],ACC         ; [CPU_] |23| /*** 32-BIT WRITE ***/

  • I understand that you need to protect your proprietary code.  But, for this issue to advance, we must reproduce it.  Please preprocess the source code that contains the problem function.  Hover your mouse over my name in the forum post.  A dialog box pops up.  Click on Send a Private Message.  A message compose box comes up.  Use the paper clip icon to attach the file.  Indicate the name of the function with the problem.

    Thanks and regards,

    -George

  • Thank you for your patience.  And thank you for sending in a test case.  I can reproduce the same output.  I agree the compiler is in error.  I filed CODEGEN-1420 in the SDOWP system to have this investigated.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George

  • Hi George,

    Checking in on status of this bug.  I see that  CODEGEN-1420 is marked as planned.  Any idea when the fix will be available?

    Thanks.

  • This bug fix has been implemented and will be in the next releases for C2000.  The 6.4.12 patch should be available within a month, and the 15.12.4.LTS patch should be available within a couple weeks.

    Please note that a status of "planned" means either that the bug fix is currently in progress or that it has been implemented but the patch hasn't been released yet.