I'm new to CCS4 and Stellaris, and am playing with an LM329B92 eval board.
1. When I first started playing with this, the code I downloaded to flash would continue to run after I exited CCS4 and restart when I turned on my PC the following morning (I.e. USB port power enabled), But now when I leave CCS4 it stops and only restarts from CCS4 with a series of actions (reload, restart, run...). Is there some control I changed to create this new behavior? This is only blinky so I haven't mucked with any boot-loader code or anything interesting (I don't think).
2. When I change my main code (alter blinky timing) and hit DEBUG, it builds and loads, but the code does not run automatically -- again I have to perform some actions (halt, restart, run). From the documentation and help screens this is not what I expect. Is this correct?
Thanks for any help -- Jim