This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Split placement on .esysmem error

The error I am getting is:

"../2837x_FLASH_lnk_cpu1.cmd", line 101: warning #10237-D: split placement (>>) ignored for ".esysmem": split run placement for this section is not permitted

I am using the default command file for the c28377D evaluation board, however I desire to specify a larger heap that 0x800.

It appeared that much of the onboard memory was unused so I changed only the below line to make use of this memory which should then allow a larger heap specification.

.esysmem : >> RAMGS2 | RAMGS3 | RAMGS4 | RAMGS5 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9 | RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 PAGE = 1

However I get this warning.

Can anyone comment on what I am not understanding that is generating this warning?  If their is a limitation of this section where is that limitation documented?

MEMORY

{

PAGE 0 : /* Program Memory */

/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */

/* BEGIN is used for the "boot to Flash" bootloader mode */

BEGIN : origin = 0x080000, length = 0x000002

RAMM0 : origin = 0x000122, length = 0x0002DE

RAMD0 : origin = 0x00B000, length = 0x000800

RAMLS0 : origin = 0x008000, length = 0x000800

RAMLS1 : origin = 0x008800, length = 0x000800

RAMLS2 : origin = 0x009000, length = 0x000800

RAMLS3 : origin = 0x009800, length = 0x000800

RAMLS4 : origin = 0x00A000, length = 0x000800

RAMGS14 : origin = 0x01A000, length = 0x001000

RAMGS15 : origin = 0x01B000, length = 0x001000

RESET : origin = 0x3FFFC0, length = 0x000002

/* Flash sectors */

FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */

FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */

FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */

FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */

FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */

FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */

FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */

FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */

FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */

FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */

FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */

FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */

FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */

FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */

PAGE 1 : /* Data Memory */

/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */

RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */

RAMD1 : origin = 0x00B800, length = 0x000800

RAMLS5 : origin = 0x00A800, length = 0x000800

RAMGS0 : origin = 0x00C000, length = 0x001000

RAMGS1 : origin = 0x00D000, length = 0x001000

RAMGS2 : origin = 0x00E000, length = 0x001000

RAMGS3 : origin = 0x00F000, length = 0x001000

RAMGS4 : origin = 0x010000, length = 0x001000

RAMGS5 : origin = 0x011000, length = 0x001000

RAMGS6 : origin = 0x012000, length = 0x001000

RAMGS7 : origin = 0x013000, length = 0x001000

RAMGS8 : origin = 0x014000, length = 0x001000

RAMGS9 : origin = 0x015000, length = 0x001000

RAMGS10 : origin = 0x016000, length = 0x001000

RAMGS11 : origin = 0x017000, length = 0x001000

RAMGS12 : origin = 0x018000, length = 0x001000

RAMGS13 : origin = 0x019000, length = 0x001000

CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400

CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400

}

 

SECTIONS

{

/* Allocate program areas: */

.cinit : > FLASHB PAGE = 0, ALIGN(4)

.pinit : > FLASHB, PAGE = 0, ALIGN(4)

.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)

codestart : > BEGIN PAGE = 0, ALIGN(4)

ramfuncs : LOAD = FLASHD,

RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,

LOAD_START(_RamfuncsLoadStart),

LOAD_SIZE(_RamfuncsLoadSize),

LOAD_END(_RamfuncsLoadEnd),

RUN_START(_RamfuncsRunStart),

RUN_SIZE(_RamfuncsRunSize),

RUN_END(_RamfuncsRunEnd),

PAGE = 0, ALIGN(4)

#ifdef __TI_COMPILER_VERSION

#if __TI_COMPILER_VERSION >= 15009000

.TI.ramfunc : {} LOAD = FLASHD,

RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,

LOAD_START(_RamfuncsLoadStart),

LOAD_SIZE(_RamfuncsLoadSize),

LOAD_END(_RamfuncsLoadEnd),

RUN_START(_RamfuncsRunStart),

RUN_SIZE(_RamfuncsRunSize),

RUN_END(_RamfuncsRunEnd),

PAGE = 0, ALIGN(4)

#endif

#endif

/* Allocate uninitalized data sections: */

.stack : > RAMM1 PAGE = 1

.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1

/*.esysmem : > RAMLS5 PAGE = 1*/

.esysmem : >> RAMGS2 | RAMGS3 | RAMGS4 | RAMGS5 | RAMGS6 | RAMGS7 | RAMGS8 | RAMGS9 | RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 PAGE = 1

/* Initalized sections go in Flash */

.econst : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)

.switch : > FLASHB PAGE = 0, ALIGN(4)

.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

Filter_RegsFile : > RAMGS0, PAGE = 1

SHARERAMGS0 : > RAMGS0, PAGE = 1

SHARERAMGS1 : > RAMGS1, PAGE = 1

/* The following section definitions are required when using the IPC API Drivers */

GROUP : > CPU1TOCPU2RAM, PAGE = 1

{

PUTBUFFER

PUTWRITEIDX

GETREADIDX

}

GROUP : > CPU2TOCPU1RAM, PAGE = 1

{

GETBUFFER : TYPE = DSECT

GETWRITEIDX : TYPE = DSECT

PUTREADIDX : TYPE = DSECT

}

}

/*

//===========================================================================

// End of file.

//===========================================================================

*/