Good morning,
I'm unable to connect to my remote BeagleBone black running Ubuntu 16.04 using Code Composer 6.1.3.00033. I've added the Linux system as described in the Linux Sitara getting started guide with ssh shell and terminal options, but when connecting I'm experiencing the following error.
Session.connect: java.io.IOException: End of IO Stream Read
I can ping and ssh into both the USB-emulated IP address and the ethernet IP address without any trouble. Interestingly, I downloaded Eclipse Neon this morning, and was able to create a remote Linux system in my remote system explorer with the same exact settings, and connect without any problems! Is this a bug within Code Composer Studio?
Thank you for your support!
Best regards,
Chris