Other Parts Discussed in Thread: CCSTUDIO
Hi all,
I am working on a project in which in the .cmd (linker) file i have made different sections.
some of these sections were referred from a library file which is included in the project.
one of those sections line is given for example below.
line 59: .text :{library_file(.text)} >> SARAM1|DARAM0|DARAM1|SARAM0|EXT0 PAGE 0
and have different sections which are from the library files which are giving same warnings.
can some one help me in debugging this warning and the error.
I am attaching the compiler warnings and errors below for your reference.
Regards,
Dinesh Davuluru
Signalogic
[Linking...] "C:\CCStudio_v3.3\C5500\cgtools\bin\cl55" -@"Debug.lkf"
<Linking>
line 59: warning:
no matching section
line 72: error:
placement fails for object ".const", size 0x27ee2 (page 0). Available
ranges:
SARAM1 size: 0x20000 unused: 0xc7bb max hole: 0xc7bb
error: section ".const" (0x0) spans page boundary: not allowed before CPU
revision 3.0