Other Parts Discussed in Thread: CODECOMPOSER
Hi
I installed CodeComposer 6.1.3 today and almost everything works fine so far. I have just a little issue:
I'm using a predefined symbol for different hardware revisions (as a compile switch):
compile option: --define=_HWREV='A'
code:
133 #if _HWREV == 'A' | _HWREV == 'B' | _HWREV == 'C'
134 cc_meas.immediate.Idc1 = IDC_SCALE * ((int16)AdcMirror.ADCRESULT0 - IDC1_OFFSET);
135 #elif _HWREV == 'D'
136 cc_meas.immediate.Idc1 = -IDC_SCALE * ((int16)AdcMirror.ADCRESULT0 - IDC1_OFFSET);
137 #else
138 #error "Unknown Hardware Revision"
139 #endif
I get the follwing error (in CCS6.1.3):
"C:/Users/sinus/SVN/CC-75-500/branches/testCCS6_1/CC75500_BIOS/headers/DriveControl/cc_measurements.h", line 133: remark #195-D: zero used for undefined preprocessing identifier "A"
"C:/Users/sinus/SVN/CC-75-500/branches/testCCS6_1/CC75500_BIOS/headers/DriveControl/cc_measurements.h", line 133: remark #195-D: zero used for undefined preprocessing identifier "A"
"C:/Users/sinus/SVN/CC-75-500/branches/testCCS6_1/CC75500_BIOS/headers/DriveControl/cc_measurements.h", line 133: remark #195-D: zero used for undefined preprocessing identifier "A"
"C:/Users/sinus/SVN/CC-75-500/branches/testCCS6_1/CC75500_BIOS/headers/DriveControl/cc_measurements.h", line 135: remark #195-D: zero used for undefined preprocessing identifier "A"
"C:/Users/sinus/SVN/CC-75-500/branches/testCCS6_1/CC75500_BIOS/headers/DriveControl/cc_measurements.h", line 138: fatal error #35: #error directive: "Unknown Hardware Revision"
I had no problem in CCS 6.1.1 .I'm using Compilier version 6.4.11.
How can I fix this?
Thank you in advance,
Simon
PS: the compile switch works with numbers but I would prefer to use chars.