I am trying to connect a Spectrum Digital XDS200, using CCS V6, on a mac. I get an error message like the following:
Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 6.0.228.0)
I do not get this error message using CCS V6 under windows.
Is there a mac OS related issue?
Thanks!