This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Updates in CCS4

Hello,

we have several pcs with CCS4 installed. On some of them we did an update of the installed features via the built in update advisor. The updates were downloaded and installed. Is it possible to download the updates only once and build an image which can be installed on all the pcs? Thus we can avoid downloading all the updates multiple times.

 

Thanks