I'm currently facing communication issues while using the SCI in TMS230F28335. The SCI is able to send data to the computer however it seems it isn't able to receive any. I wanted to check the receiver buffer of the program while it is running. Additionally I don't have the code that is currently flashed into the DSP (The code which I have is the older version of the one currently flashed into the DSP). Is there any way I can check the receiver buffer/variables while the previously flashed code is running?
I went through https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/533860 as well as http://processors.wiki.ti.com/index.php/Debug_Handbook_for_CCS but couldn't figure out how to debug the flashed code when you don't actually have the code.
I'm using a Spectrum Digital C2000 XDS510LC debug probe to connect to JTAG and running CCS 6.1.0