This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Installation 6.1.3 on Centos

Hello

we try to install centos 6.1.3 on Centos 6.5 and when we launch the .bin nothing happens. 

We try to change the mode by executing mode 

> ./ccs_setup_6.1.3.00033.bin --mode text

Error: There has been an error.
Text mode is not supported.

With this log : 

Log started 08/31/2016 at 17:17:53
Preferred installation mode : text
Trying to init installer in mode text
Mode text successfully initialized
Executing chmod -R 666 "/tmp/bitrock_installer_21453.log"
Script exit code: 0

Script output:

Script stderr:

So I try with mode xwindow

>./ccs_setup_6.1.3.00033.bin --mode xwindow

Error: There has been an error.
Text mode is not supported.

Why I cannot install? 

For information we don't use root account.