Other Parts Discussed in Thread: MSP432WARE
This is using CCS 6.2.0.00048.
Clicking on Getting Started->Browse Examples brings up the new Resource Explorer Beta which by defaults goes out to the TI Cloud (dev.ti.com/tirex). I see on the left the following:
Now I've downloaded from the main TI website. MSP432Ware_3_50_00_02 because it is the latest. There doesn't seem to be anyway to install this local package into the Resource Explorer Beta.
I can switch to classic via View->Resource Explorer Classic and I can add it via...
But that only effects what is displayed on the classic TI Resource Explorer.
I've also followed the instructions at //processors.wiki.ti.com/index.php/Resource_Explorer_Content but that also adds to the classic TI Resouce Explorer.
Letting you know that it would be nice to have a mechanism to add local resource explorer package content to the new Beta Rex.
I like it by the way.
P.P.S Also note that the current MSP432Ware is at 3.50.0.2 while the TI Cloud (Rex) has it as 3.40.0.25. Version skew.