Other Parts Discussed in Thread: CC1310, CC2650STK, ENERGIA
Hi,
Recently I've installed the latest CCS and I have difficultly starting the debug session on any CC1310 projects.
The debugger is not reaching the main function and the only thing I can do is to terminate the session:
I've used the LCD example project to see if the problem is still reproducible as you can see above. There is no error message from the debug probe. But I think the out file is not loaded because I've tried Flash Programmer 2 software and the firmware is good. Its running.
I'm using windows 10 and the example is for SmartRF06 Eva Board with XDS100v3 debug probe and TI CC1310 EM board.
Can anyone tell me what could be the problem?
Thank you and regards,
Milorad