Other Parts Discussed in Thread: SPRC097
Dear all,
I am relatively new to the DSP environment, but have spent the last 2 months playing around with it and found it is such a powerful tool.
I am currently using the Code Composer Studio version 2.12, and having trouble trying to install the F28xx On-Chip Flash Programmer.
I have installed the TMS320C2000 CCS studio 2.21 on-chip flash programmer plugin 1.12.5. But still I couldn't find it under Tools->F28xx on-chip flash programmer.
I believe this is because my CCS version is older than the 2.2x? Please correct me if I'm wrong.
If so, how can I upgrade my current CCS to 2.2x above? I have searched around to find for update patch to 2.2x but couldnt find any - is it because 2.2x is commercialised like 3.3?
I have tried another alternative solution using the SDFlash. However, I couldnt compile the project if it contains any "puts" or "printf" in it. Why wouldnt it allow me to do that? where as if I just compile and run it directly from the RAM it is fine. I just like the idea of having std output to my screen - easier to debug for me.
I would like to thank you for your help/input in advance