Hi,
We have been using CCS5.x and CCS6.x for developing our software for OMAP3 and C66x DSPs.
We check-in project files (usually .ccsproject, .cproject, .project) in workspace to our common repository.
When files are deleted from a project and the updated project files are checked in, then when other members updates their files from repository, those deleted files are still visible in CCS GUI, even though the project files don't include them. This doesn't happen always, but happens quite often.
If this happens, closing & reopening the project in CCS doesn't help. "Refreshing" the project doesn't work either.
The only way we found to correctly update the project is, deleting the project from worksapce, then re-importing the project. This workaround is OK, but one of our major annoyance.
Is there any trick to avoid this, or easier way to workaround this?
Thanks,
tamo2