Champs,
Is TI planning support for the C++11 in the C6000 DSP compiler and if yes, what is the timeline?
Thanks
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Champs,
Is TI planning support for the C++11 in the C6000 DSP compiler and if yes, what is the timeline?
Thanks
Michael
I'm also looking for C++11 support for our DSP compiler and came across this thread. I'm curious if there is partial support already or in the near future, i.e. is that why Michael was being asked about specific features of C++11? Perhaps to turn the question the other way, what features of C++11 exist in the TI compiler now or are planned for the next 12 months?
Brad Griffis said:I'm curious if there is partial support already or in the near future
No.
Brad Griffis said:is that why Michael was being asked about specific features of C++11?
No. This was just an opportunity to understand what C++11 features our customers find compelling.
Brad Griffis said:what features of C++11 exist in the TI compiler now
None.
Brad Griffis said:or are planned for the next 12 months?
Support for C++11 continues to be on our roadmap. Things are farther along than before. But we still have no firm plans to announce.
Thanks and regards,
-George