I must use CCS Version.6.0.0.00190 because of our job.
Therefore, I tried to install CCS 6.0.0.00190.exe, but I cannot install due to error occurred in installing.
Our colleagues could install this version. Our colleagues and I are using same version OS(Windows7 Pro.[32bit]).
I guess the root cause that I have installed another applications/drivers which our colleagues does not install.
However I cannot found out the root cause because I cannot understand this error means.
The detail of my encountered error is as below.
Could you help and give some advices ?
Best regards,
F.Suzuki
-----8<-----8<-----8<-----
- Error dialog message
Error: unexpected token "END" at posi...
- Detail log
unexpected token "END" at position 0; expecting VALUE
unexpected token "END" at position 0; expecting VALUE
while executing
"unexpected $tokenCursor "END" "VALUE""
(procedure "parseValue" line 5)
invoked from within
"parseValue $tokens $nrTokens tokenCursor"
(procedure "json::json2dict" line 7)
invoked from within
"json::json2dict $appsData"
(object "::jsonReader0" method "::JsonReader::parse" body line 11)
invoked from within
"parse $m_filename m_container"
while constructing object "::jsonReader0" in ::JsonReader::constructor (body line 6)
invoked from within
"JsonReader ::#auto $jsonfile"
while constructing object "::appsJson0" in ::AppsJson::constructor (body line 47)
invoked from within
"AppsJson ::#auto [[ProgramArgs::instance] override-apps-url]"
(procedure "::AppsJson::instance" body line 4)
invoked from within
"AppsJson::instance"
(object "::iSAPane0" method "::ISAPane::getSelectedApps" body line 3)
invoked from within
"getSelectedApps"
(object "::iSAPane0" method "::ISAPane::getNextStatus" body line 11)
invoked from within
"getNextStatus $numRootsSelected"
(object "::iSAPane0" method "::BaseTreePane::setNext" body line 3)
invoked from within
"setNext $numRootsSelected"
(object "::iSAPane0" method "::BaseTreePane::calculate" body line 30)
invoked from within
"calculate"
(object "::iSAPane0" method "::BaseTreePane::step" body line 4)
invoked from within
"::iSAPane0 step"
(command bound to event)