Hi folks
The code completion feature does not seem to be working at all in my current install of CCS v6.1.3.
when using the Ctrl + Space shortcut the drop-down shows "No proposals" for function parameters, even for functions defined in the same file..
No drop-down appears at all when using the operators '->' or '.' with struct names
I have thread and linked slides here https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/368991
The indexer and code completion options in my preferences are all still set to their defaults.
Is there a known issue with this or are their other settings I can try?
Thanks, T
PS: Just noticed CCs v6.2 is available, can someone that has it installed let me know if completion is working for them in it? Ta