Other Parts Discussed in Thread: TMS320F28335
I'm having problems when using pointer to a vector In CCS 6 (for C200 TMS320F28335)
I have 3 float vectors on my code, and I want to use pointers in order to work with them more efficiently , because I have a lot of index manipulation.
But I always have a lot of errors when building. Like:
line 66: error: declaration is incompatible with
"float *pentrada"
Line 66: warning: a value of type "float *" cannot be
used to initialize an entity of type "int"
pentrada = &entrada[16];
This part of the code is:
float entrada[500];
float saida[500];
float filtro[17] = {
-0.05332329190833, 0.01955569923624, 0.05182699489378, 0.0113522699158,
0.04058293444255, 0.1874313285955, 0.1582950486624, -0.1746695177164,
0.6052366278191, -0.1746695177164, 0.1582950486624, 0.1874313285955,
0.04058293444255, 0.0113522699158, 0.05182699489378, 0.01955569923624,
-0.05332329190833};
float *pentrada;
float *psaida;
float *pfiltro;
pentrada = &entrada[16]; (yes, the pointer needs to catch the address of the end of this vector)
psaida = &saida[0];
pfiltro = &filtro[0];
The errors are related to this part above ^
I've already tried:
psaida = saida;
pfiltro = filtro;
Can someone please show me where I'm going wrong?