In CCS4 using the graphing function I see the following apparent issues
(A) If I set up a graph it will work OK. If I then rebuild the code & re-execute, the graph will disappear & be replaced with a message that says "CPU Removed And/Or Terminated". The only way I can find of showing the graph then is to close the graph and recreate it via <Tools><Graph> etc.. Surely it should just continue to display the graph on rebuild?
(B) Sometimes I must exit CCS & restart to be able to get any graph shown. Sometimes the graph stops with "Unexpected Exception".
(B) With a single time graph (maybe other types too). Everytime I refresh it it will increment the X axis. E.g if there are 200 points the first plot will show the X axis 0-200, on refresh the X axis shows 200-400 etc. Should it not always show 0-200 since we are only replotting the same data set?
(C) When you save/restore a setup it does not remember the last folder used to store.
Regards --- Roger