Hi,
I have installed Eclox plugin to use Doxygen + Graphviz in the Code Composer Studio.
Now, I would like the Eclipse to automatically insert the Doxygen comment block above new functions.
I have tried the following:
1)
In Window->Preferences->C/C++->Editor,
In the right tab look for "Documentation tool comments", and in "Workspace default" set doxygen.
2)
For Project specific settings
In Project->Properties->C/C++ General:
- Tick Enable project specific Settings
- Select Doxygen as Documentation tool
But when I type "/** + Enter" above a function, Eclipse adds the following:
/**
*
*/
void test(void){
}
I as expecting something like this:
/** @brief
* @param
* @return Void.
*/
void test(void){
}
Is it possible in the Code Composer Studio?
Thank you!