This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Autocompletion uses tabs, how to force it using spaces.



Hello,

  I have configured CCS v6.1 to use spaces instead of tabs, which is under General -> Editors -> Text Editors -> Insert spaces for tabs (element checked).  The problem I am now facing is the autocomplete (e.g., when I type "if ()" with a return, press "{" then press enter once more which aligns the "{" under the "if" and places the ending "}" two lines below.  these all use tabs instead of space.) it uses tabs and not spaces.  How do I configured CCS autocomplete to use spaces and not tabs in these cases.

Regards,

Mark