This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv4.1.2.00027 crashes when Debugger started every time. Repeatable

All, I've seen several postings showing JVM errors dialog popping up. They are close to what I see, but not exactly.

WIN XP SP2; Java v6r20. Both freshly installed.

 Originally, CCSv4 would crash on start up and post the JVM error with exit code=1xxxxxxxxx. I installed Java Version 1.6.0_20, uninstalled and reinstalled ccsv4.1.2 and the startup crashes went away.

However, now every time(without fail) I start the debugger ccsv4 crashes with JVM error Exit code=1. I've tried to follow the blogs and get tips, but nothing works.

There are NO log files produced in: C:\Program Files\Texas Instruments\ccsv4\DebugServer\win32\components\Logs

Many JVM logs are produced: C:\Program Files\Texas Instruments\ccsv4\emulation\analysis\bin\hs_err_pid4060.log etc. files start out with this:

#
# An unexpected error has been detected by HotSpot Virtual Machine:
#
#  Internal Error (0xe06d7363), pid=4060, tid=3884
#
# Java VM: Java HotSpot(TM) Client VM (1.5.0_14-b03 mixed mode)
# Problematic frame:
# C  [kernel32.dll+0x12a6b]
#

---------------  T H R E A D  ---------------

Error Logs: View->Other->PDE Runtime->Error Log... shows only "A workspace crash was detected. The previous session did not exit normally"

Started ccsv4/eclipse/eclipse.exe -clean

I created a new project with nothing in it and it crashed.

Target: TMS320C5509A

EMU: SD XDS510USB

Long story short:

Start CCSV4.1.2, Load workspace, Target->Debug Active Project

JVM Error dialog Exit code=1 and subsequent options pops up and CCSv4.1.2 crashes.

Any help or insight would be greatly appreciated.