Other Parts Discussed in Thread: TLV320ADC3101
Hi All,
I am using CCS to plot FFT for an array of 24 bit data. X-axis gives me the Frequency content of the signal. I dont see an unit in the Y-Axis.
The divisions are numbered as 2.8e+6,5.7e+6 ... so on till 3.4e+7 along the Y axis
I am getting my peak at 3.4e+7. I want this to convert into dB scale or Voltage value.
1) Is this the formula -20log(Peak Val/2^23) correct??? for dBu conversion
2) Is there a setting for this in the plot?
Thanks
Lakshminarayanan