Other Parts Discussed in Thread: PGA900
Hello,
I'm currently working with the PGA900EVM and a TI Simplelink SensorTag DevPack using the latter as debugger (XDS110).
Sadly I get the Transmission Test to work (SWD) but the PGA900 Firmware doesn't debug.
I'm getting the Error 1066 0x0.
CCS is fully updated and so is the XDS110 firmware.
The problem persists even if the debugger is not connected via USB to the PC, so i guess it's a driver related issue.
Could you confirm that ?
I know I'm supposed to use the XDS200 but I gave it a try with the in-house debugger.
Thanks in advance
Daniele