Other Parts Discussed in Thread: CCSTUDIO
Hi, I recently tried to install CCStudio v3.1 for my c6713 DSK board and my F2812 eZdsp board on the same computer and found out that I am not able to have both installed at the same time. So I have decided to only keep the CCStudio v3.1 for the c6713 DSK board on my computer, seeing that is used in the project I am currently working on now.
I have as far as I can tell uninstalled everything that is associated with CCStudio and tried to reinstall the drivers and CCStudio v3.1 for the c6713 DSK board. The install seem to go fine, and I can even use the 6713 DSK Diagnostic utility and get a passing mark. However when I try and launch CCStudio using the “6713 DSK CCStudio v3.1” icon I get the following error pop up window:
Your Code Composer does not support the connected target. Device driver name: “C:\CCStudio_v3.1\drivers\sdgo6713dsk.dvr” and then CCStudio closes out.
I had Code Composer working fine before I tried to install the drivers and files for the F2812 eZdsp board. Is it possible that there is a conflict between the drivers of both DSP’s and they never were fully uninstalled or is there some thing else that I would need to do to get back to a working CCStudio of the c6713 DSK board?
Thanks