Hi,
I'm getting this type of errors, Please help me to solve this problem. I'm doing a project on cc430f5137 by installing CCS v6.2.0 in linux(ubuntu) 64-bit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm getting this type of errors, Please help me to solve this problem. I'm doing a project on cc430f5137 by installing CCS v6.2.0 in linux(ubuntu) 64-bit.
Your project attempts to combine object files built with different file formats. All of the libraries and object files must use the same file format. Older versions of the MSP430 compiler used COFF. Newer versions use EABI. Since COFF format is going away, you need to identify which files or libraries are built for COFF, and change them to EABI.
For more background on this error, please see this wiki article. For general background on object file formats, please see this wiki article.
Thanks and regards,
-George