Hi
I have been working on a prgram on CAN bus with my LM3S8962 MCU kit. The program which I was trying was an example program given along with the software CD. While compiling the program I got the following errors.
unresolved symbol UARTprintf, first referenced in ./simple_tx.obj sid line 0 1278823057808 20
unresolved symbol UARTStdioInit, first referenced in ./simple_tx.obj sid line 0 1278823057807 19
I am sure that I have included the header for UARTprintf and the utilities files for UART StudioInit. I specifically mentioned the path for those two files, but still it dint work.
I dint tamper with the header files or with the utilities file in the CD.
What could be the possible solution for this problem.