This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V4 not connecting with target

Other Parts Discussed in Thread: TMS320C5515

Hi everyone,

I have got a TMS320C5515 eZdsp USB stick. I have installed CCS 4.0. Everything was working fine till yesterday and I could connect to my target DSP USB stick. Yesterday when I connected the board and tried to to connect the target I am getting the following error in a sepeerate window.

Error connecting to the target:
Error 0x80002240/-121
Fatal Error during: Initialization, OCS, Control,

I am not able to see the whole error message too. I could not understand or figure out the error. After my initial installation I did upgrade the software many times. So I thought that there is some problem with the CCS. I uninstalled it and reinstalled it again. I am getting the same error again.

Can anyone help me out in this.

I used "XDS100 USB emulator" in connection type, and "USBSTK5515" from devices list and saved it as the target configuration. (Also the sequence of 4 LEDS in the board are glowing alternatively from the moment I connect it to my PC without stopping)

I wish it is not a case of my hardware got bad.

ANy help or suggestion or further clarification will be much appreciated.

Krish.