This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug : Flash Programmer: Error encountered when writing to flash memory

Hello,

I have some issues using debug on Code Composer Studio v6.2.0.00050  (windows 7 64 bits pro service pack 1).

I'm working on the Delfino f28335 (f28335 control card R2.2 on docking station usb emu r3).

The debug used to work, but it doesn't flash the tms anymore.

When I try to debug and load the program, ccs6 tries to launch something like 2 debug sessions.

It's erasing and writing to the flash at the same time.

I got :

C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: C:\******\FLASH.out: Load failed.

I reinstalled all code composer studio v6.2, my drivers are up to date and the JTAG test in target configuration works.

I tried to figure out why the last days, but I didn't find anything.

Any help will be appreciated.

Mathieu

Screen of a debug session :