This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gmake: *** [tiescappl.o] Error 1



Hi!

Recently I have bought the TMDSICE3359 for testing purposes, however I've been unable so far to run anything but the default demo code. I am using CCS 6.2.0 in which I have tried the EtherCAT Slave example code (the second one that can be downloaded here, found under sysbios_ind_sdk_02.01.02.02\sdk\examples\ethercat_slave) but I cannot get the am335x debug code to build properly.. I've gotten rid of many of the errors at start, but I'm left with some errors that I do not understand:

gmake: *** [tiescappl.o] Error 1
gmake: *** [tiescutils.o] Error 1
gmake: Target 'all' not remade because of errors.
recipe for target 'tiescappl.o' failed
recipe for target 'tiescappl.o' failed

Any ideas on how to resolve this issue? These errors are very undescriptive..

  • That error comes from gmake, and has nothing to do with the TI toolset; it merely means that some rule in your Makefile produced a failing exit status. You will need to look backwards in the log for another error. If you can't find it, please post the entire output of the gmake command.