Because of the holidays, TI E2E™ design support forum responses may be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARM TI code generation tools: armofd.exe truncates long names

Hi,

I am running the command: armofd.exe --obj_display=none,sections Dem_Client.o

code generation tools: ti-cgt-arm_5.2.5\bin

But I notice that the sections names are truncated when it reaches a certain length.
Please see the sample output below.

How can I display the full text of the section name without converting the output into XML?


Copied from Command Prompt
====================================================================
arm\bin>armofd.exe --obj_display=none,sections Dem_Client.o

OBJECT FILE:  Dem_Client.o

 Section Information

    id name                      load addr  run addr    size align alloc
    -- ----                      ---------  --------    ---- ----- -----
     0 (no name)                 0x00000000 0x00000000   0x0     0   N
     1 .text                     0x00000000 0x00000000   0x0     2   Y
     2 .data                     0x00000000 0x00000000   0x8     4   Y
     3 .bss:Dem_TxData           0x00000000 0x00000000 0x120     2   Y
     4 .text:Dem_SetEvStatusF... 0x00000000 0x00000000  0x3c     4   Y
     5 .text:Dem_SaveErrorPre... 0x00000000 0x00000000  0x90     4   Y
     6 .text:Dem_ReportErrorS... 0x00000000 0x00000000  0x48     4   Y
     7 .text:Dem_GetEventIdValid 0x00000000 0x00000000  0x38     2   Y
     8 .text:Dem_SetEventStatus  0x00000000 0x00000000  0x30     4   Y
     9 .text:Dem_ResetSlaveEv... 0x00000000 0x00000000   0xc     4   Y
    10 .text:Dem_InitHwErrors    0x00000000 0x00000000  0x10     4   Y
    11 .text:Dem_InitPreExtData  0x00000000 0x00000000  0x28     4   Y
    12 .text:Dem_PreInit         0x00000000 0x00000000  0x58     4   Y
    13 .text:Dem_TaskSlaveEve... 0x00000000 0x00000000  0x40     4   Y
    14 .text:Dem_MainFunction    0x00000000 0x00000000  0x1c     4   Y
    15 .text:Dem_Init            0x00000000 0x00000000  0x1c     4   Y
    16 .ARM.attributes           0x00000000 0x00000000  0x58     0   N
    17 .symtab                   0x00000000 0x00000000 0x780     0   N
    18 .rel.text:Dem_SetEvSta... 0x00000000 0x00000000  0x18     0   N
    19 .rel.text:Dem_SaveErro... 0x00000000 0x00000000  0x30     0   N
    20 .rel.text:Dem_ReportEr... 0x00000000 0x00000000  0x28     0   N
    21 .rel.text:Dem_GetEvent... 0x00000000 0x00000000   0x8     0   N
    22 .rel.text:Dem_SetEvent... 0x00000000 0x00000000  0x20     0   N
    23 .rel.text:Dem_InitHwEr... 0x00000000 0x00000000  0x10     0   N
    24 .rel.text:Dem_InitPreE... 0x00000000 0x00000000  0x10     0   N
    25 .rel.text:Dem_PreInit     0x00000000 0x00000000  0x58     0   N
    26 .rel.text:Dem_TaskSlav... 0x00000000 0x00000000  0x38     0   N
    27 .rel.text:Dem_MainFunc... 0x00000000 0x00000000  0x18     0   N
    28 .rel.text:Dem_ResetSla... 0x00000000 0x00000000   0x8     0   N
    29 .rel.text:Dem_Init        0x00000000 0x00000000  0x10     0   N
    30 .TI.symbol.alias          0x00000000 0x00000000   0x9     0   N
    31 .TI.section.flags         0x00000000 0x00000000  0x1a     0   N
    32 .strtab                   0x00000000 0x00000000 0x665     0   N
    33 .shstrtab                 0x00000000 0x00000000 0x310     0   N