HI,
I am using CCS 6_1_3 on a mac pro, with a 432 launchpad and see no resume button, though I do see a terminate button.
Basically, the project worked a few months back, I put down this project to go work on other things while waiting for a board with the 432 TI chip to be built, then when I came back to verify my baseline before continuing, I got the no resume button problem.
I tried the workaround identified in the related posting, i.e. deleting the configuration and restarting, but it didn't help.
I also tried the 432 on smaller project (supplied w/CCS) on the mac and can get the smaller project to run.
I also have a Windows 7 laptop CCS version 6_2_0 and see the resume button and can run the project.
Is this a mac only problem?
thanks,
bob s.