This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs 3.1 install problem

Other Parts Discussed in Thread: CCSTUDIO

hi

i have installed ccs3.1 on windows 7.

but when i run it...it gives following error

 

"Problem signature:

  Problem Event Name: APPCRASH

  Application Name: cc_app.exe

  Application Version: 5.90.0.227

  Application Timestamp: 428571e4

  Fault Module Name: ntdll.dll

  Fault Module Version: 6.1.7600.16385

  Fault Module Timestamp: 4a5bdadb

  Exception Code: c0000005

  Exception Offset: 0002fc47

  OS Version: 6.1.7600.2.0.0.256.1

  Locale ID: 1033

  Additional Information 1: 4c0d

  Additional Information 2: 4c0d4d78887f76d971d5d00f1f20a433

  Additional Information 3: 4c0d

  Additional Information 4: 4c0d4d78887f76d971d5d00f1f20a433"

 

Please help

  • Hi Amir,

    Please provide more information on your environment. See the forum readme for more details on what information we are looking for:

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/3131.aspx

    Thanks

    ki

  • hi

    => version of host os:

    Windows 7 ultimate

    version 6.1 (Build 7600)

    Copyright 2009, Microsoft coorporation


    => Exact version number for IDE:

    code composer studio v3.1.3.1.19.0


    =>Exact target:

    TMS320C6713 Rev B


    => Error when ccs3.1 crash is:

    Problem signature:

      Problem Event Name: APPCRASH

      Application Name: comp_mgr.exe

      Application Version: 5.90.0.227

      Application Timestamp: 428568d8

      Fault Module Name: MFC42.DLL

      Fault Module Version: 6.6.8063.0

      Fault Module Timestamp: 4a5bda30

      Exception Code: c0000005

      Exception Offset: 000261bd

      OS Version: 6.1.7600.2.0.0.256.1

      Locale ID: 1033

      Additional Information 1: 0a9e

      Additional Information 2: 0a9e372d3b4ad19135b953a78882e789

      Additional Information 3: 0a9e

      Additional Information 4: 0a9e372d3b4ad19135b953a78882e789

    Read our privacy statement online:

      http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

    If the online privacy statement is not available, please read our privacy statement offline:

      C:\Windows\system32\en-US\erofflps.txt




  • Amir Shafiq said:

    => version of host os:

    Windows 7 ultimate

    version 6.1 (Build 7600)

    Copyright 2009, Microsoft coorporation

    Is this 32-bit or 64-bit?

    Amir Shafiq said:

    =>Exact target:

    TMS320C6713 Rev B

    Which emulator are you using?

    Amir Shafiq said:

    => Exact version number for IDE:

    code composer studio v3.1.3.1.19.0

    This is the original release of 3.1. There has been many service release updates to 3.1 since then. Can you update to the latest service release (I believe 3.1.30 is the latest)? You can get to it from CCS Update Advisor. After updating, can you see if the issue still exists?

    Also, do you see an crash dump files?

    http://processors.wiki.ti.com/index.php/CCStudio_FAQ#Q:_What_are_these_.2A.dmp_files_generated_by_CCStudio_.282.30.2B.29.3F

    Thanks

    ki

     

  • One more question: Are you using a DSK version of CCS? Basically are you using a limited CCS version that came with a C6713 DSK? If so, then you may not be able to update that version.

  • hi ki

    it is 32 bit windows

     

    i also have DSK, but currently i am running simulator for tms320c6713

    it is

    c6713 device cycle accurate simulator ,little endian

     

    yes this is original version.. i no update option is availble

     

    no *.dmp files are present in <CCStudio Install Directory>\cc\bin\Logs

    Also i have searched in c:\

    but couldnt find any *.dmp file for ccs

    Best regards

    Amir Shafiq

  • Amir,

    CCS 3.1 is very old and no longer supported. Because you have a limited version, you cannot take any of the 3.1 patches which may have a fix that would have addressed your issue.

    Would you be willing to try moving to CCSv4? It does come with the 6713 Device Cycle Accurate Simulator (both endianness) and if you will be using the simulator, you can use one of the licensing options which lets you use the simulator without any cost. You will have a learning curve since CCSv4 is very different from CCSv3 but because we really can't support you with your limited CCS 3.1 install, I think this is your best option.

    ki

  • Thanks

    I will move to ccsv4, From where i can download it. It subscribed to it. But its link expired

  • hey dude....ccs3.1 won't run on windows7 make sure ur system has  windows2000/XP.

  • ccs3.1 works on windows 2000/XP..it won't run on windows7. or install ccs4 on windows 7.