Other Parts Discussed in Thread: CCSTUDIO
Dear Tech Support,
I am running Windows 10 Version 1607
OS Build 14393.447
i7-2600 CPU
16.o GB of RAM
64-bit OS
Currently installed are the following version of Code Composer Studio
Code Composer Studio Version: 6.2.0.00050
Code Composer Studio Version: 6.1.0.00104
Code Composer Studio Version: CCS 5.5.0
In the lower right corner of the startup screen, it states "Full License"
Problem:
When running version 6.2.0.00050, I cannot create a new project.
After the "New CCS Project" window pops up,
the "Target:" line is blank, and
IT WILL NOT ALLOW ME TO ENTER EITHER ALPHA OR NUMERICAL DATA.
Also:
on the "Getting Started" page
Clicking on the video, starts the video, however clicking
on the "FULL SCREEN" ICON does not work.
Is there a conflict between my different version of CCS?
(from the PROPERTIES window for each of the three startup ICONS)
Version: 6.2.0.00050
Target: C:\ti_v6\ccsv6\eclipse\ccstudio.exe
Start in: C:\ti_v6\ccsv6\eclipse
Version: 6.1.0.00104
Target: C:\ti\ccsv6\eclipse\ccstudio.exe
Start in: C:\ti\ccsv6\eclipse
Version: CCS 5.5.0
Target: C:\ti\ccsv5\eclipse\ccstudio.exe
Start in: C:\ti/ccsv5/eclipse
If I have a conflict between these different version,
do I need to uninstall a version and reinstall?
Any and all help will be greatly appreciated
Thanks,