Hi
I am looking for some support regarding InstaSPIN_F2806xM_UNIVERSAL (guicomposer).
I can run InstaSPIN_F2806xM_UNIVERSAL with my DRV8312-69M-KIT without any issues on a single hardware setup. I know that during initialization its connects to the target hardware and flashes the ControlCARD. I have no problem doing these things on single setup.
I would like to be able to run InstaSPIN_F2806xM_Universal on multiple DRV8312-69M-KIT at the same time. Is there a way to tell the InstaSPIN_F2806xM_Universal software during Target initialization to use a specific COM PORT for communication?
I am using a powered USB Hub with 2 x DRV8312-69M-KIT) in my setup. Both DRV8312 (ControlCard 069) get turned on (power) at the same time. The PC detects the COM Port on the computer. The issue is that the InstaSPIN_F2806xM_Universal GUI does not know which device to initialize.
Below is the error I get during initialization.
Restarting Program Model...
Initializing target : C:\ti\guicomposer\eclipse\workspace\.metadata\.plugins\com.ti.binding.program\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Debug Probe/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
Is there anyway to tell the Universal GUI software which debug com port to use for initialization?
A quick response is highly appreciated.
Thanks in advance.