This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am currently running CCS4.0.1 , BIOS 5.40.02.22, on a DM648. I am trying to get the CPU load, but the graph does not display anything. As a matter of fact, nothing on the RTA shows anything. Only ROV populates any data.
I enabled Real Time Analysis and All TRC Trace Event Classes.
One strange thing (maybe?) that I see is when I open the RTA control panel. The four vertical options have check marks on them (LOG_system, CPU Load, etc), but vertical options don't even show the check box.
Any thoughts?
Thank you in advance.
Alin
Hi Ki,
Just updated to CCS4.2.4 and the BIOS is now at 5.41.10.36.
I still have the same problem.
Alin