This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bootable application not work with latest compiler

My application booted just fine before the new compiler (19.9.0.LTS) .  I notice this when I had to develope on another computer and started getting warnings.

It seems to compile OK but can't link the boot.obj from rts2800.ml.lib:

The cmd file looked like this previously for that section:

.boot > BEGIN
{
-l rts2800_ml.lib<boot.obj>(.text)
}

To get it compile I had to add the page to it (no big deal):

.boot > BEGIN PAGE = 0
{
-l rts2800_ml.lib<boot.obj>(.text)
}

But now I get a warning that there is no matching section for "-l rts2800_ml.lib<boot.obj>(.text)"

It still compiles but the first 50 bytes are blank so the program crashes...  

It seems the program needs this section to start properly as I have moved the rest of the code to start there and it fails...

I'll be going back to the original compiler in the mean time, but I would like to know how to fix this in the future... or point out a bug if it exists in the new compiler.

Also, note that I can run the program just fine from the debugger without that section... I just can't run my boot loader and start the application code anymore.

Thanks,

Kyle

  • Kyle,

    Thanks for bringing this to our attention. I'll move your post to the Compilers Forum for better feedback.

    Elizabeth
  • I don't know what is going on.  Please attach the linker command file to your next post.  So the forum will accept it, add the file extension .txt to it.  After seeing that, I might be able to explain what is happening.  At a minimum, I will be able to ask better questions.

    Thanks and regards,

    -George

  • /*
     * Copyright (c) 2013, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    /*
     *  ======== TMS320F28032.cmd ========
     *  Define the memory block start/length for the F28032
     */
    
    /* 
     *  PAGE 0 will be used to organize program sections
     *  PAGE 1 will be used to organize data sections
     *
     *  Notes: 
     *        Memory blocks on F2803x are uniform (ie same
     *        physical memory) in both PAGE 0 and PAGE 1.  
     *        That is the same memory region should not be
     *        defined for both PAGE 0 and PAGE 1.
     *        Doing so will result in corruption of program 
     *        and/or data. 
     *        
     *        L0 memory blocks are mirrored - that is
     *        they can be accessed in high memory or low memory.
     *        For simplicity only one instance is used in this
     *        linker file.
     */
    
     _Cla1Prog_Start = _CLAfuncsRunStart;
    -heap 0x200
    -stack 0x200
    
    // Define a size for the CLA scratchpad area that will be used
    // by the CLA compiler for local symbols and temps
    // Also force references to the special symbols that mark the
    // scratchpad are.
    CLA_SCRATCHPAD_SIZE = 0x100;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
    	//OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
    	//FLASHH      : origin = 0x3F0000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHG      : origin = 0x3F1000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHF      : origin = 0x3F2000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHE      : origin = 0x3F3000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHD      : origin = 0x3F4000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHC      : origin = 0x3F5000, length = 0x000FFF     /* on-chip FLASH */
    	//FLASHB      : origin = 0x3F6000, length = 0x000F7F     /* on-chip FLASH */
    	BEGIN       : origin = 0x3E8000, length = 0x000050     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
    	FLASH_PROG	: origin = 0x3E8050, length = 0x00CFAD		//,	fill = 0xFFFF
    	FLASH_CLA	: origin = 0x3F4FFD, length = 0x000FFF		//,	fill = 0xFFFF
    	CHECKUM		: origin = 0x3F5FFD, length = 0x000002		//Where the code checksum is stored.
    	//FLASHA      : origin = 0x3F7000, length = 0x000F7F     /* on-chip FLASH */
    	//CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
    	//BEGIN       : origin = 0x3F6FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
    	//CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
    
        IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
        IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
        IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA	   /* IQ Math Tables in Boot ROM */
    
        //ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
        RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
        //VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
        //L0SARAM_COPY	: origin = 0x3F8000, length = 0x000800     /* A check to make sure Program flash doesn't overlap in this section */
    
    	L3SARAM     : origin = 0x009000, length = 0x000FFF,	//fill = 0xFFFF    /* RAM Reserved for CLA */
    
    PAGE 1 :   /* Data Memory */
    
        M01SARAM    : origin = 0x000000, length = 0x000800, //fill = 0x0000    /* FAST RAM on-chip RAM block M0, M1 */
        //PIEVECT     : origin = 0x000D00, length = 0x000100
        //L0SARAM    	: origin = 0x008000, length = 0x000800     /* SLOWER RAM on-chip RAM block L0 */
        L01SARAM    : origin = 0x008000, length = 0x000C00
    	//L0_SARAM	: origin = 0x3F8000, length = 0x000800
    	//CLARAM0     : origin = 0x008800, length = 0x000400
        CLARAM1     : origin = 0x008C00, length = 0x000400
    
    	CLA_CPU_MSGRAM  : origin = 0x001480, length = 0x000080 /* CLA-R/W, CPU-R message RAM */
    	CPU_CLA_MSGRAM  : origin = 0x001500, length = 0x000080 /* CPU-R/W, CLA-R message RAM */
    
    
    }
    
    /*
     *  Allocate sections to memory blocks.
     *  Note:
     *      codestart   user defined section in DSP28_CodeStartBranch.asm
     *                  used to redirect code execution when booting to flash
     *
     *      ramfuncs    user defined section to store functions that will be
     *                  copied from Flash into RAM
     */ 
    
    SECTIONS
    {
        /* Allocate program areas: */
        .cinit              : > FLASH_PROG       PAGE = 0
        .pinit              : > FLASH_PROG       PAGE = 0
        .text               : > FLASH_PROG       PAGE = 0
    
        codestart           : > BEGIN       PAGE = 0
        .boot > BEGIN PAGE = 0
    	{
        	-l rts2800_ml.lib<boot.obj>(.text)
    	}
    
    
        ramfuncs            : LOAD = FLASH_PROG      PAGE = 0,
                              RUN  = M01SARAM   PAGE = 1,
                              LOAD_START(_RamfuncsLoadStart),
                              LOAD_SIZE(_RamfuncsLoadSize),
                              LOAD_END(_RamfuncsLoadEnd),
                              RUN_START(_RamfuncsRunStart)
    						//{  //Used for SFRA library but something seems off, so it's commented out for now...
    						//			--library=rts2800_ml.lib<fs_mpy.obj>
    						//			--library=SFRA_IQ_Lib.lib<SFRA_IQ_INJECT.obj>
    						//			--library=SFRA_IQ_Lib.lib<SFRA_IQ_COLLECT.obj>
    						//}
    
    	controlfuncs        : LOAD = FLASH_PROG      PAGE = 0,
                              RUN  = L01SARAM   PAGE = 1,
                              LOAD_START(_ControlfuncsLoadStart),
                              LOAD_SIZE(_ControlfuncsLoadSize),
                              LOAD_END(_ControlfuncsLoadEnd),
                              RUN_START(_ControlfuncsRunStart)
    
    
    
       /*
        CLATables        	: LOAD = FLASH_CLA      PAGE = 0,
                              RUN  = CLARAM1   PAGE = 1,
                              LOAD_START(_CLATablesLoadStart),
                              LOAD_SIZE(_CLATablesLoadSize),
                              LOAD_END(_CLATablesLoadEnd),
                              RUN_START(_CLATablesRunStart)
    	{
        CLA1mathTables
        .const_cla
        }
    	*/
        //csmpasswds          : > CSM_PWL     PAGE = 0
        //csm_rsvd            : > CSM_RSVD    PAGE = 0
    
        /* Allocate uninitalized data sections: */
        .stack              : > M01SARAM 		PAGE = 1 // | L03SARAM      //PAGE = 1
        .ebss               : > L01SARAM 		PAGE = 1 //| L03SARAM      //PAGE = 1
        .esysmem            : > L01SARAM		PAGE = 1 //| M01SARAM      //PAGE = 1
        .cio                : > M01SARAM		PAGE = 1 //| M01SARAM      //PAGE = 1
    	.reset              : > RESET,      PAGE = 0, TYPE = DSECT
    
        /* Initalized sections go in Flash */
        /* For SDFlash to program these, they must be allocated to page 0 */
        .econst             : > FLASH_PROG       PAGE = 0
        .switch             : > FLASH_PROG       PAGE = 0
        .args               : > FLASH_PROG       PAGE = 0
    
        /* Allocate IQ math areas: */
        IQmath              : > FLASH_PROG       PAGE = 0            /* Math Code */
        IQmathTables        : > IQTABLES    PAGE = 0, TYPE = NOLOAD
    
    	//HWI and SWI runtime sections:
    	RuntimeSection		: > M01SARAM 	PAGE = 1
    
    	//SFRA Section:
    	SFRA_IQ_Data 		: > L01SARAM, ALIGN = 64, PAGE = 1
    
    	//Control Sections:
    	ControlVariables	: > CPU_CLA_MSGRAM	PAGE = 1
    	ReponseVariables    : > CLA_CPU_MSGRAM	PAGE = 1
    	CNTL_2P2Z_Coef		: > CPU_CLA_MSGRAM	PAGE = 1
    	CNTL_3P3Z_Coef		: > CPU_CLA_MSGRAM	PAGE = 1
    	CNTL_2P2Z_Var		: > CLA_CPU_MSGRAM	PAGE = 1
    	CNTL_3P3Z_Var		: > CLA_CPU_MSGRAM	PAGE = 1
    	ADCDRV_4ch_Section	: > M01SARAM	PAGE = 1
    	PWMDRV_NIFC_Section	: > M01SARAM	PAGE = 1
    	CNTL_3P3Z_Section	: > M01SARAM	PAGE = 1
    	CNTL_2P2Z_Section	: > M01SARAM	PAGE = 1
    	PWMDRV_1chHiResUpDwnCnt_Section		: > M01SARAM	PAGE = 1
    
    	//ISR-Functions:
    	Net_terminals		: > L01SARAM	PAGE = 1
    
    	//SENSBus Stuff:
    	SENS_Bus_Dev_Info		: > L01SARAM	PAGE = 1
    	SENS_Bus_Charger		: > M01SARAM 	PAGE = 1
    	SENS_Bus_Charger_EE		: > L01SARAM 	PAGE = 1
    	Charger_Alarms			: > L01SARAM 	PAGE = 1
    
    	//Modbus Stuff:
    	MODBUS_Lookup_Table     : > M01SARAM    PAGE = 1
    
    	//CAN_FIFO stuff:
    	CAN_FIFO_buffer			: > M01SARAM 	PAGE = 1
    
    	//Control Sections:
    	FLASH_API_Section	: > M01SARAM	PAGE = 1
    
    	//Data Logger
    	CrankAnalyzer		: > L01SARAM 	PAGE = 1
    
    	//CLA section:
    	//CLA_Prog			: > L3SARAM 	PAGE = 1
    	Cla1Prog        	: LOAD = FLASH_CLA
                              RUN  = L3SARAM
                              LOAD_START(_CLAfuncsLoadStart),
                              LOAD_SIZE(_CLAfuncsLoadSize),
                              LOAD_END(_CLAfuncsLoadEnd),
                              RUN_START(_CLAfuncsRunStart)
                              PAGE = 0
    
    	GROUP	           : LOAD = FLASH_CLA       PAGE = 0,
                             RUN = CLARAM1   		PAGE = 1,
                             LOAD_START(_CLATablesLoadStart),
                             LOAD_SIZE(_CLATablesLoadSize),
                             LOAD_END(_CLATablesLoadEnd),
                             RUN_START(_CLATablesRunStart)
    						   {
    						    CLA1mathTables
    						    .const_cla
    						   }
    
    	Cla1ToCpuMsgRAM   : > CLA_CPU_MSGRAM PAGE = 1
       	CpuToCla1MsgRAM   : > CPU_CLA_MSGRAM PAGE = 1
    
    	//Cla1DataRam0		   : > CLARAM0,		  PAGE = 1
        Cla1DataRam1		   : > CLARAM1,		  PAGE = 1
    
    
    
    
        CLAscratch          :
                             { *.obj(CLAscratch)
                             . += CLA_SCRATCHPAD_SIZE;
                             *.obj(CLAscratch_end) } > CLARAM1,
    					     PAGE = 1
        /*
         *  Uncomment the section below if calling the IQNexp() or IQexp()
         *  functions from the IQMath.lib library in order to utilize the 
         *  relevant IQ Math table in Boot ROM (This saves space and Boot ROM 
         *  is 1 wait-state). If this section is not uncommented, IQmathTables2
         *  will be loaded into other memory (SARAM, Flash, etc.) and will take
         *  up space, but 0 wait-state is possible.
         */
        /*
        IQmathTables2       : > IQTABLES2   PAGE = 0, TYPE = NOLOAD
        {
            IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
        }
        */
    
        /*
         *  Uncomment the section below if calling the IQNasin() or IQasin()
         *  functions from the IQMath.lib library in order to utilize the
         *  relevant IQ Math table in Boot ROM (This saves space and Boot ROM
         *  is 1 wait-state). If this section is not uncommented, IQmathTables2
         *  will be loaded into other memory (SARAM, Flash, etc.) and will take
         *  up space, but 0 wait-state is possible.
         */
        /*
        IQmathTables3       : > IQTABLES3   PAGE = 0, TYPE = NOLOAD
        {
            IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
        }
        */
    }