This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simultaneously connect two TM4C123GXL Launchpads to one instance of CCS v6?

I would like to simultaneously have two, or possibly more, TM4C123GXL Launchpads connected to one instance of CCS v6.  I intend to work on each Launchpad individually, each running different and unrelated code.

When both are simultaneously connected to USB ports on my PC I can see them in them Device Manager; each has its own related “Stellaris ICDI DFU Device” and “Stellaris ICDI JTAG/SWD Interface”, and com port assigned.  They function in CCS v6 individually when only one of them is connected.

My question: Is there a method to switch between them from within one instance of CCS v6?

Suggestions will be appreciated.

Thanks, Bob