This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650: Stack overflow Errror when opening a project

Part Number: CC2650

Tool/software: Code Composer Studio

Hallo,

when opening an project file I get always the following error:

Unhandled event loop exception
java.lang.StackOverflowError

I am using Code Composer Studio  Version: 6.2.0.00050

Regardes

Matthias

  • Matthias Geiger said:

    when opening an project file I get always the following error:

    Unhandled event loop exception
    java.lang.StackOverflowError

    Do you see the error during project import? Or after closing and then opening a project?
    Would you be able to zip up and attach the project here for us to take a look at?

  • Hi,

    I have the problem with any project I try to open. Also with example projects from TI and with imported projects from CCS6.1 which will be already in CCS6.1 ok!


    It happend suddenly after working in a project that have been compiled several times bevor.

    Perhaps this could be a problem with the CCS6.2 installation and not with the project files.

    Best regardes

    Matthias

  • Matthias Geiger said:
    Perhaps this could be a problem with the CCS6.2 installation and not with the project files.

    It sounds like that might be the case. Could you please try uninstalling and reinstalling CCS? If installing to the same directory, please be sure to completely delete the directory with the previous installation before reinstalling.