Part Number: CC3200MOD
Other Parts Discussed in Thread: UNIFLASH, CC3200, CC3100
Tool/software: Code Composer Studio
We are working out our EOL process using Uniflash and it doesn't seem to work so well. I'm using a variant of the example in the CC3200 Production Line Guide:
C:)cd
C:\ti\uniflash_3.4\ccs_base\scripting\examples\uniflash\cmdLine
C:)uniflash -config "C:\Users\ANONYMOUS\tidla_sn04.usf -spPath="C:\ti\CC3100_CC3200
_ServicePack_1.0.1.6-2.7.0.0" -operations format servicePackUpdate program
***** Texas Instruments Universal Flash Programmer *****
<START: 12:23:58 GMT-0500 (EST)>
js: "C:\ti\uniflash_3.4\ccs_base\scripting\examples\uniflash\cmdLine\uniFlash_co
re.js", line 8: uncaught JavaScript runtime exception: TypeError: Cannot call me
thod "setDefaultDialogResponse" of null
That ain't so good. This is with a fresh install of Uniflash 3.4. The config file is one I regularly use from the Uniflash GUI. What gives? Did I miss something in the setup?
Thx,
Dallas