This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: CCS6.x license for K2G EVM emulation using XDS2xxUSB

Thanks for the extended help. I want to respond that this works/doesn't work, but I can't seem to load the program onto the board. According to the wiki instructions, I'm supposed to select "TI XDS2xxUSB Debug Probe", which I guess means that there's no onboard debug probe. Which means I have to buy a full CCS license (or choose the "evaluation" license option).

However, when I try to create an evaluation key, the site linked below just times out. Am I correct in my assumptions/steps? Do I have to buy the full CCS license for the EVMK2G board?  Is there another link to grab an evaluation license?

Edit: the link has been fixed.  Thank you.

www.ti.com/.../productactivation.tsp