This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: absolute symbol "_RamfuncsLoadEnd" being redefined

Part Number: TMS320F28379D
Other Parts Discussed in Thread: CODECOMPOSER, CONTROLSUITE

Tool/software: Code Composer Studio

When building my project with CodeComposer Studio, I get the following warning :

absolute symbol "_RamfuncsLoadEnd" being redefined

Other symbols are being redefined as well : _RamfuncsLoadSize, _RamfuncsLoadStart, _RamfuncsRunEnd, _RamfuncsRunSize, _RamfuncsRunStart.

When executing the code, I stepped into the code where there is a copy of time critical and Flash setup code to RAM (in function InitSysCtrl); 0 bytes are copied since RamfuncLoadSize is set to 0.

Compiler Version : TI v16.9.1.LTS

controlSUITE version : v3.4.1

Linker command file : 2837xD_FLASH_lnk_cpu1.cmd

Thank you,