Part Number: TMS320F28069M
Tool/software: Code Composer Studio
When I run the InstaSPIN Universal GUI the splash screen comes up and then the program exits without any notification. I have uninstalled it and reinstalled it several times to no avail. I have also contacted the InstaSPIN folds and they said it looked like an install problem and sent me your way. Here are a few observations.
1) OS: Windows 10
2) Hardware: Launchpad XL 28069
3) XDS100 channel A and B are present in the device manager, but the serial port is not
4) In looking at the install log some of the components return a non-zero value, but the install program itself reports things were installed OK.
Here is a snipit from the install log
******************************************
Script stderr:
Program ended with an error exit code
Error running D:\ti/guicomposer/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "D:\ti/guicomposer/ccs_base/emulation/windows/xds100_drivers/ftdi" : Program ended with an error exit code
[10:27:02] Running XDS560 Driver Installer
Executing D:\ti/guicomposer/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "D:\ti/guicomposer/ccs_base/emulation/windows/xds560_drivers"
Script exit code: 256
Script output:
Script stderr:
Program ended with an error exit code
Error running D:\ti/guicomposer/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "D:\ti/guicomposer/ccs_base/emulation/windows/xds560_drivers" : Program ended with an error exit code
[10:27:03] Running XDS2xx Driver Installer
Executing D:\ti/guicomposer/ccs_base/emulation/windows/DPInst64.exe /SE /SW /SA /PATH "D:\ti/guicomposer/ccs_base/emulation/windows/xds2xx_drivers"
Script exit code: 256
*******************************************
I would greatly appreciate any help as this has completely crippled our ability to evaluate your product for our pressing motor control needs.
Thanks!